AnsweredAssumed Answered

Questions about the FSLBOT

Question asked by robots on Nov 30, 2012
Latest reply on Dec 4, 2012 by Kevin C Anderle

Hi,

     I recently got a FSLBOT and I have been having difficulties setting it up properly.  I have been trying to get it working with Robotsee as i want to use it in conjunction with a webcam, which seemed impossible to do with stickOS as far as i have found. If this is not true, can anyone point me in the right direction for achieving this with stickOS?  However, when running the robotsee example code for the FSLBOT, the fslbotopen() function doesn't manage to properly connect to the FSLBOT.  I have tried doing this while plugged in  both USB ports with no success. 

     One possibility for this problem i came up with is that i previously tried to use stickOS, which may have changed some of the settings on the robot, making robotsee not work properly.  However, i am not sure how to properly reset the robot to fix that  if that is the case.

 

If anyone could help me out, i would appreciate it.

Outcomes