AnsweredAssumed Answered

Problems debugging with CW10.2

Question asked by Marcos Guasch on Nov 23, 2012
Latest reply on Dec 5, 2012 by Marcos Guasch

Hi all,

 

I have started working with CW10.2 (running under Windows 7 - 64 bit) a few weeks a go and when debugging I found several problems that I cannot solve. First one is that when I click the 'Reset' icon, the program counter jumps to random positions instead of going to main() as I configured. Second one is that if I set a breakpoint in one of the source files, the debugger does not stop. However, breakpoints work properly in other source files in the same project. Finally, sometimes after stopping (Suspend) the program execution, when I click 'Step into' again, the debugger does not execute a single instruction, but continues running as if I click 'Resume', but then I cannot stop it again. After this, I have to 'Terminate' debugger, clean and build project again.

Thanks in advacne for your kind help.

Marcos

Outcomes