TWRK20D72M Warrings: Launch configuration is a migration candidate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWRK20D72M Warrings: Launch configuration is a migration candidate

Jump to solution
879 Views
miniwang
Contributor III

The environment is [MQX3.8.1] & [CW10.2].

When I new a MQX 3.8 project and select "TWRK20D72M" board to be used, there are 3 warrings .

(This problem is also occured for "TWRK40D100M" board.)

1.jpg

|Deseciption:

|    Launch configuration is a migration candidate

|Resource:

|    MQX_twrk20d72m_hello_twrk20d72m_Int_Flash_Debug_PnE U-MultiLink.launch

|    MQX_twrk20d72m_hello_twrk20d72m_Int_Flash_Release_PnE U-MultiLink.launch

|    MQX_twrk20d72m_hello_twrk20d72m_Int_RAM_PnE U-MultiLink.launch

When I use Quick Fix to fix it, there is a failed message.

2.jpg

|RSE Migration Failed

|Reason:

|Migration failed for unknown system "K20DX256M7"

Does any one have the same problem as well?

What is the impact of this warring?

p.s I don't have TWRK20D72M so I can't download and debug it.

    Next week I will get our custom board use MK20DN512ZVLL10, so that I creat a custom BSP and project for it in advance.

Thank you in advance.

Mini


0 Kudos
1 Solution
423 Views
c0170
Senior Contributor III

Hello Mini Wang,

here's infocenter's link to read about migration. this warning is just a notification:

http://www.freescale.com/infocenter/index.jsp?topic=%2Fcom.freescale.doc.fsl_eclipse_ext_guide%2Fdoc...

There's subchapter  Display of Launch Configurations Needing Migration which explains how to suppress the warnings.

Regards.

MartinK

View solution in original post

0 Kudos
2 Replies
424 Views
c0170
Senior Contributor III

Hello Mini Wang,

here's infocenter's link to read about migration. this warning is just a notification:

http://www.freescale.com/infocenter/index.jsp?topic=%2Fcom.freescale.doc.fsl_eclipse_ext_guide%2Fdoc...

There's subchapter  Display of Launch Configurations Needing Migration which explains how to suppress the warnings.

Regards.

MartinK

0 Kudos
423 Views
miniwang
Contributor III

Thank you very much, MartinK.

It's seems not a issue if it's just a notification and doesn't impact anything.

Mini

0 Kudos