AnsweredAssumed Answered

How should I make IMX53 processor run at full speed.

Question asked by Swaraj vutturi on Nov 20, 2012
Latest reply on Nov 23, 2012 by Vladan Jovanovic

Hi,

 

I have a application, which runs very slow on IMX53 ubuntu 10.04. To meet my requirements I should run processor at high speed, so that it processes my SDIO device faster.

 

What should I do to make processor run at very speed?

 

I'm already running the SDIO at higher clock speed (50MHz), but still that is not sufficient for me to process. Currently IMX processor is running at 300MHz, So I thought of increasing this processing speed by running processor at higher speed.

 

Can anyone help me in running the SDIO device at higher speed to achieve desired result.

 

Thanks

Swaraj


Outcomes