How do I set the stack size in a project using CodeWarrior 10? Other IDEs that I've used have a setting in the project options to do this, but there doesn't seem to be one for CW10. Is there a file somewhere that needs to be modified? Thanks.
Solved! Go to Solution.
Typically this is in the linker file. The syntax depends from toolchain (well linker) to another, so it is little bit different say for gcc compared to the Freescale compilers.
For Processor Expert enabled project: there is a setting in the CPU component properties > build tab for this.
Hope this helps,
Erich
Typically this is in the linker file. The syntax depends from toolchain (well linker) to another, so it is little bit different say for gcc compared to the Freescale compilers.
For Processor Expert enabled project: there is a setting in the CPU component properties > build tab for this.
Hope this helps,
Erich
Thanks!