i.MX28evk sd boot faults

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28evk sd boot faults

Jump to solution
900 Views
chris321
Contributor IV

Hello everyone,

I'm trying to create a bootable SD card as descriped in the LTIB_for_i.MX28__a_step-by-step_guide .

I've tried the following steps with a fresh freescale-ltib-ubuntu vm-image.

* start the terminal in LTIB directory

* ./ltib

    Elapsed: 1 seconds

    Build Succeeded (ltib is preconfigured by freescale)

* mk_mx_28 /dev/sdb

    confirmed with yes and entered password for madfsl

    [...] Done! Plug the SD/MMC card into the i.MX board and power-on.

   

alright so far..

but if I boot the i.MX28 evk from this SD card I got errors.

Sometimes:

Uncompressing Linux...

invalid compressed format (err=2)

-- System halted

and sometimes

Uncompressing Linux...

incomplete literal tree

-- System halted

But if I rename the imx28_ivt_linux.sb to imx28_linux.sb and overwrite the file in the ~ltib/rootfs/boot folder and execute the mk_mx28_sd script again than the evk starts without any faults.

So I'll think there is something missing in the ltib configuration, but I have no idea what.


Labels (2)
0 Kudos
1 Solution
632 Views
chris321
Contributor IV

It seems to be caused by the by default activated secure boot. I think a note about this in the step by step guide would be very usefull.

View solution in original post

0 Kudos
1 Reply
633 Views
chris321
Contributor IV

It seems to be caused by the by default activated secure boot. I think a note about this in the step by step guide would be very usefull.

0 Kudos