SPI example for ADC like the TWR-ADCDAC-LTC for Keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI example for ADC like the TWR-ADCDAC-LTC for Keil

Jump to solution
1,832 Views
tfrauenrath
Contributor III

Hi there,

I´ve got 2 questions regarding SPI communication under MQC with ADC´s:

1.) Is there any example for the TWR-ADCDAC-LTC Board together with K60 Board for Keil µVision?

2.) Is there any example to communicate with an Analog Devices ADC´s like the AD719x (AD7190/AD7191/AD7192) under MQX (which I can convert to µVision...)?

I think the routines under the SPI example are not helpful because the cover only memory transfers....

Thanks a lot!

0 Kudos
1 Solution
861 Views
DavidS
NXP Employee
NXP Employee

Hi Tobias,

From the top level http://www.freescale.com/tower web site you can find the product page for the TWR-ADCDAC-LTC Tower card.

This is vendor supported so the last update I see is for MQX3.7 and only using CW IDE and IAR.

Regards,

David

View solution in original post

0 Kudos
2 Replies
861 Views
tfrauenrath
Contributor III

Oh, I also found these documents. I think Keil support is something new and Keil users are always one step behind...

862 Views
DavidS
NXP Employee
NXP Employee

Hi Tobias,

From the top level http://www.freescale.com/tower web site you can find the product page for the TWR-ADCDAC-LTC Tower card.

This is vendor supported so the last update I see is for MQX3.7 and only using CW IDE and IAR.

Regards,

David

0 Kudos