Inter Processor Communication in PSC 9131 not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inter Processor Communication in PSC 9131 not working

1,804 Views
saad
Contributor I

Hi all,

I am working with PSC9131 RDB board in CW for SC-10.2.9

A sample demo application was given for inter processor communication named "IPC integration". I have downloaded the application onto the board into SC3850 core and executed it.

It (SC3850 core) enabled a hardware semaphore and then went on an infinite loop. I think it is expecting the e500 core to release the hardware semaphore, which was not occurring.

I want to know how this sample application really works? Am I missing anything while running this code?

Any help in this regard is much appreciated.

Thanks.

Saad

Labels (1)
0 Kudos
2 Replies

1,379 Views
mattsm
Contributor III

What SDK for this product are you using? Are you using the u-boot, Linux, device tree, and root file system from this SDK or just trying to use the example IPC application by itself?

0 Kudos

1,379 Views
saad
Contributor I

Hi Mathew,

As explained in my query I am just trying to use the example application "IPC integration" only. Please help in this regard.

Thanks

0 Kudos