For some reason, the P&E debugger won't download when I enable trace/software analysis. I get a "An internal error occurred during...." error message. At startup, I'm always greeted with "There is a mismatch between the System environment and the workbench environment, which may result in Software Analysis malfunctioning." I suspect that this is the case. Has anyone seen this one before? Any solution? Any idea where to look?
Perhaps and environment variable is whacked?
Hello,
Windows or Linux host? Which version (10.2 or 10.3)?
Have you just installed a service pack or an update? I have seen such a thing if I do a 'restart' of Eclipse instead of closing it and then start a fresh one.
Not sure, but it could be related to the LD_LIBRARY_PATH (or similar). Could you check/post the content of your cwide-env file (located in the eclipse folder) and check if all the paths exist on your system?
I hope this helps,
Erich
Erich,
That would be Linux (Mageia 32-bit), CW10.2. I'll check my cwide-env file later this evening.
I just checked it on WinXP, CW10.2, and was able to run one analysis.
Bob