i.MX53 Embedded-Qt-4.7.0 touchscreen wrong points positions and events

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Embedded-Qt-4.7.0 touchscreen wrong points positions and events

536 Views
leroy_o
Contributor III

I am using a Sabre platform for i.MX53 with a LVDS1 LCD / touchpanel, with tslib.

When using Embedded-Qt-4.7.0 applications that make use of the cursor position, when I tap on the screen, sometimes, the cursor moves at a location distant from the point where I tap. Also there are two mouse events mouseButtonpressed, instead of one when the application behaves correctly in this case.

Recalibrating the touchscreen doesn't solve the problem.

This problem occurs only on Embedded-Qt-4.7.0 applications. The output of "hexdump /dev/input/event0" is correct. So this is not a low level issue.

Have someone experienced the same with Embedded-Qt applications, and solved it?

Labels (3)
0 Kudos
0 Replies