AnsweredAssumed Answered

THE TIME CONSUMPTION FROM THE TSEC TO THE CORE THROUGH DPAA

Question asked by fang XIAO on Oct 22, 2012
Latest reply on Apr 16, 2013 by lunminliang

Is there any reference about the delay from TSEC to the core? I know that the accurate time consumption varies from the number of the existing work queues and the tasks which DPAA must do. However, it is useful to know the approximate level of delay when a single package (there is no other tasks in DPAA) is transmitted from the input of the TSEC to the e500 core, because in our communication system this delay is a sensitive parameter. It decides that whether a package can be delivered to the e500 core from the ethernet before the deadline time.

Outcomes