Application stucking on iMX51 + Qt4.7.3 + simplegl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application stucking on iMX51 + Qt4.7.3 + simplegl

789 Views
antoninobattagl
Contributor I

Hi All,

     I am developping a commercial system using iMX51 + Qt 4.7.3 + simplegl driver.

The application uses opengl 32 bits. System has 256 MB of RAM used with the following bootloader prms:

gpu_memory=128M gpu_nommu

The application (called APP) is using opengl only in for 2 animation involving crossfading, bluring and brightness.

The vertex and fragment shader are very simple and are written inside 2 qml files.

Sometimes the application stucks with the following output:

APP: /u/build/nightly_build/build/ltib/rpm/BUILD/amd-gpu-src-11.05.01/driver/build/linux/mx51/../../../es20/src/gl2_framebufferobject.c:388: set_framebuffer: Assertion `0' failed.

I dont know the reason why. Does anybody know what is the meaning of this message?

Have you experienced this issue?

Any support is very appreciated. Thx.

Labels (2)
0 Kudos
3 Replies

524 Views
imxcommunitysco
Senior Contributor II

Antonino, this DI will be closed if no response from your in 3 days.

Thanks,

Yixing

0 Kudos

524 Views
YixingKong
Senior Contributor IV

Antonino, FSL engineer is working on your questions now and needs your answer for further investigation. Please respnd as soon as possible.

Thanks,

Yixing

0 Kudos

524 Views
andre_silva
NXP Employee
NXP Employee

Do you only see issue when using a QT based application ?

regards,

Andre

0 Kudos