AnsweredAssumed Answered

Can Zstar3 usb stick  be replaced by 1322x NSK-DBG kit USB dongle  in order to function with zstar sensor accelerometers

Question asked by Adam azam on Oct 16, 2012
Latest reply on Oct 19, 2012 by Joshevelle

Hi all,

I am working on a project in which we are using zstar3 usb stick to work with zstar3 accelerometers. Proper hardware description is given in the link:

http://cache.freescale.com/files/sensors/doc/fact_sheet/ZSTAR3BOARDFS.pdf

we need  to use 1322x-usb dongle instead of zstar3 usb dongle.  I want to receive accelerometer signals at 1322x-USB dongle side.  In the case of Zstar3 we have library there but here we do not have any class, library or any other com-port receiver abstraction layer where we can easily receive data at the 1322x-usb dongle side.

Can somebody suggest where to look for the relevant material.   Any help would be appreciated.

Regards

Cyber

Outcomes