AnsweredAssumed Answered

Can't debug TWR-K20D72M

Question asked by dtno on Oct 11, 2012
Latest reply on Oct 11, 2012 by dtno

Hi,

 

I'm new to Freescale (so, new to MQX, CW, TWR, etc.). We just received our programmer (P&E Micro Multilink Universal) and I need to test it on our TWR module.

 

I'm using CW10.2, MQX 3.8.1, Win 7 64bits

 

To do so, I created a MQX 3.8 project using the Taskq sample. I build without problems. Then, when I try to debug the application, I get an error saying that my project doesn't have a connection configured. I can confirm that by opening the Run->Debug Configurations...

 

I created other MQX projects for a ColdFire MCU (which we will also use) and the "Connection" is created by the project. Not for the TWR one.

 

Can anyone help me with that? It's kind of critical, it will influence our choice of the MCU for our next board...

 

Thanks !

Outcomes