Hello,
I am trying to setup the EIM of an i.MX53(MX535) to access both a Fujitsu FRAM (MB85R1002) and an FPGA. I cannot access either. The address bus is de-multiplexed by a 74LCX16373 transparent latch driven by EIM_CS0. I observe erratic address values on the address bus. The documentation is not helping much, there are no examples of asynchronous multiplexed timings in the reference manual.
Has anyone had luck in setting such a configuration up ?
For info, I tried the following setups, none work :
EIM_CS0WCR1 = 0x16002082, 0x16002682, 0x1F0C2E92
EIM_CS0RCR1 = 0x16000202 , 0x16000502, 0x1F034522
Regards.
Would you mind to send me this part of schematic to review? If you don't want to show the schematic here, please submit a SR for this issue.
Hello Jimmy, the confusion arose due to inconsistent documentation in the i.MX53 UG manual :
25.3.3 Multiplexed Address/Data Mode
In this mode, multiplexing addresses and data bits on the same pins is supported for
synchronous/asynchronous accesses to x8/x16/ x32 data width memory devices.
For more information about the pins that drive data/address in 8/16/32 non-muxed mode
and 16/32 muxed mode, refer to the EIM Internal Module Multiplexing table in the EIM
Internal Pads Allocation chapter of the datasheet.
In fact, do as you want, x8 bits mode does not work in multiplexed mode...
Regards.