Good low-cost debugger for Kinetis K & L-series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Good low-cost debugger for Kinetis K & L-series

Jump to solution
847 Views
estrack
Contributor II

What's a good choice for a low-cost ($100 to $300) debugger for the Kinetis K series, that should also support the L series?

Needs to work with CodeWarrior 10.2 / 10.3


I suspect OSBDM from EBay is an option, but perhaps slow, as it is used on the tower boards (?), or CYCLONEMAX_PE, but it is $900, or perhaps PnE U-Multilink, but it has caveats as to which versions of CodeWarrior support it?


What do most of you professional devs use for debugging K series micros?

Labels (2)
0 Kudos
1 Solution
511 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

View solution in original post

0 Kudos
1 Reply
512 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

0 Kudos