Hi,
I am trying to get the eGUI mqx demo to work with TWR-LCD on TWR-K60N512. The baremetal project works fine but then when I build the MQX project on 3.8.1 it does not work. It is configured to use SPI2 and the correct SW1 switches are set however I don't see any display on the LCD.
I probed the clk, data and they seem to look fine. However, the CS is not changing. I have not made any changes to affect the Chip Select. Did anyone get this eGUI mqx demo for N512 to work on MQX 3.8.1 and CW 10.2?
I would really appreciate your input as I have already spend a lot of time trying to debug it.
Thanks!
Did you ever find an answer to this?
Hello,
I bring this up just to see if you have proceeded further with your problem or not? Share with us :smileywink:
Regards,
MartinK