AnsweredAssumed Answered

BSP default_IO_channel using multilink

Question asked by khoanguyen on Sep 24, 2012
Latest reply on Sep 26, 2012 by David E Seymour

I was wondering what is the correct BSP default_IO_CHANNEL setting, if you are using the PEmicro USB multilink to debug rather than the on-board

OSJTAG. The default setting was at "ttyf" but since the board is no longer plugged in to my computer (power is being used through a mini-USB wall powered adapter).

 

I'm using the mutex example to test.

I've tried changing the configuration to "iodebug" but I've been getting the random print_tasks. Adding in the "_time_delay" function helped but then the tasks were ran randomly instead of round robin.

 

I've also checked the user_config.h file and the MQX_TIME_SLICE is enabled and added.

 

 

Since the PE mircro MultiLink is connected via USB serial, what is the correct IO channel setting when you are using an external JTAG?

 

Thanks,

 

Khoa Nguyen

Outcomes