I.MX53 SABRE Tablet boot up using Linux 3.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX53 SABRE Tablet boot up using Linux 3.1

1,177 Views
Shri1z
Contributor I

Has anybody booted i.mx53 sabre tablet using linaro linux 3.1 kernel?

The default source does not build. After patching from the 2.6.35 source, the kernel builds, but stalls while booting up with following status:

[1.134983] Waiting for root device /dev/mmcblk0p2...
[1.203537] mmc0: host does not support reading read-only switch. assuming write-enable.
[1.311426] mmc0: new SDHC card at address e624
[1.316441] mmcblk0: mmc0:e624 SU08G 7.40 GiB
[1.324020]  mmcblk0: p1 p2
[1.469814] EXT4-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
[1.582402] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[1.590680] VFS: Mounted root (ext4 filesystem) on device 179:2.
[1.600274] Freeing init memory: 272K
[2.325943] mmc2: new high speed MMC card at address 0001
[2.332683] mmcblk1: mmc2:0001 SEM08G 7.39 GiB
[2.337804] mmcblk1boot0: mmc2:0001 SEM08G partition 1 1.00 MiB
[2.344391] mmcblk1boot1: mmc2:0001 SEM08G partition 2 1.00 MiB

modprobe: FATAL: Could not load /lib/modules/3.1.1+/modules.dep: No such file or directory

[   12.379638] mmc2: Timeout waiting for hardware interrupt.

[   12.385414] mmcblk1: error -110 sending stop command, original cmd response 0x900, card status 0x400900

[   12.404516] mmcblk1: error -110 transferring data, sector 15003648, nr 8, cmd response 0x900, card status 0x0

[   12.431452] mmcblk1: retrying using single block read

[   12.443436] mmcblk1: error -84 transferring data, sector 15003648, nr 8, cmd response 0x900, card status 0x0

[   12.469754] end_request: I/O error, dev mmcblk1, sector 15003648

[   12.485180] mmcblk1: error -84 transferring data, sector 15003649, nr 7, cmd response 0x900, card status 0x0

Can anybody help me to resolve this error?

Labels (2)
0 Kudos
3 Replies

533 Views
Mats1z
Contributor III

Dear Shri,

I have booted linux 2.6.32 in sabre tablet. Now I need linux 3.0 or higher running in my system. Will you please share the steps you followed in bringing up sabre tablet with linux 3.1.

Thanks

Mathews Paul

0 Kudos

533 Views
fabio_estevam
NXP Employee
NXP Employee

I would suggest you to try the latest stable kernel (3.5.3).

Regards,

Fabio Estevam

0 Kudos

533 Views
Mats1z
Contributor III

Hi Fabio,

Can you suggest the steps involved in bringing up sabre tablet with latest stable kernel. Please suggest a good tutorial for the same.

Thanks

Mathews Paul

0 Kudos