AnsweredAssumed Answered

52235 Internal Flash Speculation Address Qualification Incomplete?

Question asked by je rosell on Sep 12, 2012
Latest reply on Sep 12, 2012 by TomE

Hello I'm working with M52235EVB and Codewarrior 7.2. I'm having an exception which seems to be the address speculation error.

It's solved with the workaround 1, and if I debug the exception both flash and ram addresses match (see the picture).

But in the chip errata document I read:

 

This erratum is fixed in devices labeled with the A suffix or 3M23E mask.


I've checked my device and it's labeled

PCF52235CAG60

M23E

QAA0550

 

Is that A in red the suffix mentioned in the errata document or it should be PCF52235CAG60A?

 

Thank you

Attachments

Outcomes