about i.mx6q boot question. -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about i.mx6q boot question. -blog archive

536 Views
tom_y
Contributor I

I want boot i.mx6q_arm2 from sd,I use 4GB DDR3,8chip,BSP is L3.0.15_12.05.01.

question:

1:system no boot when Temperature less than 43 C.(CPU is PCIMX6Q6AVT10AB)

boot logs:

  U-Boot 2009.08 ( 8鏈?10 2012 - 18:44:25)

  U-Boot code: 27800720 -> 27831000 BSS: -> 278664B4
  CPU: Freescale i.MX6 family TO0.0 at 792 MHz
  Temperature: 60 C, calibration data 0x5874de7d

   .......

2:4GB DDR3 only find 2GB(BANK 1,DDR3 type is EDJ4216BASE )

 I modify mx6q_arm.h 

  #define CONFIG_NR_DRAM_BANKS      2

  #define PHYS_SDRAM_1                      CSD0_DDR_BASE_ADDR

  #define PHYS_SDRAM_1_SIZE             (2u*1024*1024*1024)

  #define PHYS_SDRAM_2                      CSD1_DDR_BASE_ADDR

  #define PHYS_SDRAM_2_SIZE             (2u*1024*1024*1024)

  #define iomem_valid_addr(addr,size) \

                       ((addr>=PHYS_SDRAM_1 && addr<=(PHYS_SDRAM_1+PHYS_SDRAM_1_SIZE)) \

                       || (addr>=PHYS_SDRAM_2 && addr<=(PHYS_SDRAM_2+PHYS_SDRAM_2_SIZE)))

boot logs:  

   Board: MX6Q/SDL-ARM2:[ POR ]
   Boot Device: SD
   I2C: ready
   RAM Configuration:
   Bank #0: 00000000 0 kB
   Bank #1: 00000000 0 kB
   RAM Configuration:
   Bank #0: 10000000 2 GB
   Bank #1: 00000000 0 kB

What is cause?  please help me, thanks!

Tags (1)
0 Kudos
0 Replies