Hey,
I am performing ltib build operation as shown in the step 4 in section 2.2 in the document that i have attached.
but this error is coming
"ltib can not run because one or more host packages needed to run it are either missing or out of date or not in ltib's standard path" .
i am a newbie :( ..can any one help me ?
Here's some info here:
http://www.imxdev.org/wiki/index.php?title=ALL_Boards_ltib_config_ubuntu
Make a mental note of this step though -> "Ubuntu distro uses dash instead of bash as shell, then change it to bash:", it probably won't hurt you, but there are some differences in scripting across the two shells.
But either way, I followed the instructions exactly, then ltib worked fine.
-Randy
look in the error log!