I found weird behavior of the LVDS.
Only reasonable explanation is that LDB_CTRL bits 5 and 6 are exchanged.
Another possible typo in the document is description of bit_mapping_ch0:
0 Use SPWG standard.
1 Use JEIDA standard.
I found that VESA (I believe that the same as SPWG) LVDS display works properly if the bit_mapping_ch0 is set.
After modification of the bits definition the color on the 18 bpp LCD of Touch Revolution became proper.
Thanks, Vladan.
Done
Hi,
If you believe there's an error in documentation, please enter a Service Request to Freescale via www.freescale.com/support
Regards,
Vladan
Document that probably has typos is:
i.MX53 Multimedia Applications
Processor Reference Manual
Document Number: iMX53RM
Rev. 2, 12/2011
The Kernel code definitions are the same as in the document.