I'm running the Ubuntu from the SD card delivered with the i.MX53 QSB (i.e. Lucid, kernel version 2.6.35.3-1129-g691c08a).
I cannot mount samba shares from command line. No problem accessing same shares from nautilus (file manager).
ddd@iMX53:~$ sudo mount.cifs //192.168.0.1/P_Drive /mnt/netdrv/
[sudo] password for ddd:
Password:
mount error: cifs filesystem not supported by the system
mount error(19): No such device
Refer to the mount.cifs(8) manual page (e.g. man mount.cifs)
It appears cifs kernel module is missing
ddd@iMX53:~$ sudo modprobe fuse
FATAL: Module fuse not found.
ddd@iMX53:~$ ll /lib/modules/`uname -r`/kernel/fs
total 8.0K
drwxr-xr-x 2 root root 4.0K 2011-10-07 05:21 autofs4/
drwxr-xr-x 2 root root 4.0K 2011-10-07 05:21 nls/
Has anyone come across this issue? I'd expect to see cifs.ko in '.../kernel/fs' directory. How can I add this module?
Thanks,
Dejan