Yuri Petriaev

CW for ColdFire 6.4, target MCF5307, two last bytes of s19 file cut off, is it alignment?

Discussion created by Yuri Petriaev on Jun 15, 2007
Latest reply on Jun 18, 2007 by CrasyCat
I have two last bytes of the binary being cut off while programming device.
The max S-record length is set to 25 characters.
The last line of the binary data is shorter then the rest of the source.
 
===== Example =======
.....
S319000FFFE07C14FE01FF06FE01FF0CFE01FF1CFE01FF28FE011B
S319000FFFF4FF32FE01FF36FE01FF8CFE020012FE027CE2FE0285
S313001000087CD4FE027C0C000D7248000D72585E
S70500040010E6
 
Is this an alignment issue?
How can I correct it?
Please see attached lcf file (mainboard.txt).

Outcomes