Ed Sutter

LTIB build problems on UBUNTU

Discussion created by Ed Sutter on Jul 6, 2012
Latest reply on Jul 9, 2012 by Ed Sutter

Hi,

I'm just getting started with i.MX53 QSB.  I have a machine dedicated for the iMX53 builds that I installed UBUNTU DESKTOP 12.04 LTS.  I then pulled down


L2.6.35_11.09.01_ER_source_bundle.tar.gz from the


i.MX53 Software and Development Tool Resources page and I *believe* I followed the instructions as outlined on http://www.imxdev.org/wiki/index.php?title=All_Boards_LTIB and http://www.imxdev.org/wiki/index.php?title=ALL_Boards_ltib_config_u... .  

Attempting to run ltib -c at that point caused an error that indicated that zlib was not available even though it was installed.  I found information at this site:

http://theembeddedsystems.blogspot.com/2011/11/install-ltib-in-ubun...

That got me over that hump, and tried ltib -c again.

I get the following error:

Installing host support packages.

This only needs to be done once per host, but may take up to
an hour to complete ...

If an error occurs, a log file with the full output may be found in:
/home/els/imx53/ltib/host_config.log

Exiting on error or interrupt
Please see >> /home/els/imx53/ltib/host_config.log for details


and the host_config.log file says:

rpmdb: --force-debian: unknown option
Died at ./ltib line 2341.
traceback:
 main::setup_rpmdb:2341
  main::check_rpm_setup:2404
   main::host_checks:1424
    main:542

Started: Fri Jul  6 11:24:33 2012
Ended:   Fri Jul  6 11:24:34 2012
Elapsed: 1 seconds

Build Failed

Seems like this is more trouble than it should be.  Has anyone built LTIB on the latest UBUNTU or am I just doing something wrong?

Outcomes