Hi,
I bought IMX6 evaluation kit and was able to boot evaluation board with SD Card provided in the package. After that I tried to put my own u-boot.bin and uImage on the SD Card to verify it boots properly.
I get following error when I boot.
In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:19:b8:00:e9:e9
FEC0 [PRIME]
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
mmc0(part 0) is current device
MMC: block number 0x1 exceeds max(0x0)
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
** Bad partition 1 **
mmc1 is current device
reading /6q_bootscript
** Unable to read "/6q_bootscript" from mmc 1:1 **
Loading file "/6q_bootscript" from mmc device 1:1 (xxb1)
** File not found /6q_bootscript
I am looking where can I find this 6q_bootscript file. As I lost the default image on SD card is there a way to recover this image? I searched on freescale website but did not find any documentation for this.
Regards,
Sumit
I was able to boot this board after installing back these missing files. This is closed now.
Regards,
Sumit