patrick immling

set ethernet address on usb0

Discussion created by patrick immling on May 4, 2012

Hi All,

 

I have an imx51 evk board. I have the freescale android image running on it(R.10.3).

 

I have two DHCP networks. I have one normally connected over ethernet port of the board. The other via usb port. How do I set the MAC address in my U-boot command?

 

I did a normal setenv ethaddr xx.xx.xx.xx.

 

However both the ethernet and usb0 seem to be polling their respective dhcp servers without reply.

Can the ethaddr overwrite the previous addresS?

 

How can I get the two dhcp-based network interfaces runing?

 

Please help

Outcomes