I just upgraded my board from 16Mbyte-8bit FLASH to 64Mbyte-16bit FLASH (S29GL512N). I can not get it to boot, has anyone else tried booting from this size flash?
My boot jumpers are set to: non-mux, 16bit data, no swap, Max wait, 0x100 boot exception, Large_fl selected, most_graphics not selected.
My config changed as follows:
BOOTSTR: from-FF00 to-FC00
CSBOOTCR: from-00047800 to-00047D00
The interesting thing is that with the CodeWarrior USB-TAP I can burn and verify the flash. But when I try to execute, or inspect flash I get garbage.
The biggest question is: Has anyone booted in LARGE FLASH mode?
Thanks in advance for your reply.