Hello!
Where can I get description for write u-boot on NAND? I do not use Windows in work and, I think, can't use Mfgtool.
Thank you and exuse me my bad english.
Hello!
Where can I get description for write u-boot on NAND? I do not use Windows in work and, I think, can't use Mfgtool.
Thank you and exuse me my bad english.
Sorry, we do not have tools to burn NANDs via serial (UART / USB) port for i.MX53 under host Linux.
Basically one can use abilities of internal i.MX53 serial bootloader (to design own loaders) - please look
at Florent's discussion :
http://imxcommunity.org/group/imx53quickstartboard/forum/topics/serial-download-example-instructions-or-tool?commentId=4103961%3AComment%3A64643&xg_source=msg_com_gr_forum
Another problem - it is needed to support special NAND boot structures (FCB, DBBT), described in i.MX53 RM,
section 7.5.2 (NAND Flash).
This is not good. May be I can get description on protocol, then I can try write flasher? I can see source Mfgtool, but this is not very simple way.
Yuri Muhin said:
Another problem - it is needed to support special NAND boot structures (FCB, DBBT), described in i.MX53 RM,
section 7.5.2 (NAND Flash).
I think i.MX53 must can booting from NAND.
As for the serial protocol - it is described in section 7.8.3 (Serial Download Protocol)
of i.MX53 RM. Also please look at the enclosed - as an example - sorry- for windows
Brilliantov Kirill Vladimirovich said:
This is not good. May be I can get description on protocol, then I can try write flasher? I can see source Mfgtool, but this is not very simple way.
Yuri Muhin said:Another problem - it is needed to support special NAND boot structures (FCB, DBBT), described in i.MX53 RM,
section 7.5.2 (NAND Flash).I think i.MX53 must can booting from NAND.
Hi Yuri,
Does Mfgtool support NAND flashing, partitioning etc? Our cutomized board is based on iMX53 QSB but uses NAND as boot device other than microSD card. That brings in some overheads to figure out how to program initial u-boot and create partition on NAND.
Yuri Muhin said:
Sorry, we do not have tools to burn NANDs via serial (UART / USB) port for i.MX53 under host Linux.
Basically one can use abilities of internal i.MX53 serial bootloader (to design own loaders) - please look
at Florent's discussion :
http://imxcommunity.org/group/imx53quickstartboard/forum/topics/ser...
Another problem - it is needed to support special NAND boot structures (FCB, DBBT), described in i.MX53 RM,
section 7.5.2 (NAND Flash).
You may use SD to boot Linux, which should include kobs-ng utility.
Then :
kobs-ng init --chip_0_device_path=/dev/mtd0 u-boot.bin