Hello I have just started working with QT and the i.MX28EVK.
I have the kernel working and have, finally, compiled the QT libraries using this discussion: http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx28?commentId=4103961%3AComment%3A...
None of the demos are running all of them give me the error:
./fluidlauncher: error while loading shared libraries: libQtGui.so.4: cannot open shared object file: No such file or directory
I have located the file in question in the directory /home/madfsl/Software/QtEmbedded-4.7.4-imx/lib
I have tried 'export export LD_LIBRARY_PATH=/home/madfsl/Software/QtEmbedded-4.7.4-imx/lib'
But no success.
What am I missing?
Thank you very much, now my board work fine.
Thanks for your advice!
Yes it turns out that I when I copy the files to the SD card they need to be in the exact same directory under home that they were complied in. Then everything works.
Hi Richard,
have you solved the problem?