FTDI Android D2XX Driver Errors on android i.MX53 QSB :Consumer closed input channel or an error occurred. events=0x8 & Channel is unrecoverably broken and will be disposed!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTDI Android D2XX Driver Errors on android i.MX53 QSB :Consumer closed input channel or an error occurred. events=0x8 & Channel is unrecoverably broken and will be disposed!

799 Views
admin
Specialist II

Dear All,

 

I'm using the below android application when i run the below sample application when i click the data button after typing the data

 

 

On clicking the Info button in the sample application is not displaying the number of devices it is coming out  of that application,

 

And when i clicked the  Data button is not writing  the text from the edit box to the device, & not even reads any available data back for displaying below the Data button. even after a loopback connector was fitted so the data received is the same as the data sent.

  

The above android application usage is provided in the TN_134 FTDI Android D2XX Driver pdf

(you can get this in google by searching this key word)

  

when i run the above application i getting the below errors

 

E/InputDispatcher(2176): channel '2b10d600 com.ftdi.d2xx/com.ftdi.d2xx.D2XXSampleActivity (server)' ~ Consumer closed input channel or an error occurred.  events=0x8

 

 

E/InputDispatcher(2176): channel '2b10d600 com.ftdi.d2xx/com.ftdi.d2xx.D2XXSampleActivity (server)' ~ Channel is unrecoverably broken and will be disposed!

 

 

As am new to this android applns development could any body pls help me in how to fix this problem or could any correct the above problem in the above code n share the same with me

 

Kindly do the needful as soon as possible,

 

Advanced Thanks,

Srinivasan S

Labels (1)
0 Kudos
0 Replies