SAIF2 interrupt on iMX233 (WINCE6 R3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAIF2 interrupt on iMX233 (WINCE6 R3)

398 Views
MenM
Contributor I

Hi,

I try to get SAIF2 up and running on a iMX233. I see that the DMA command complete interrupt is set after a DMA transfer, but my thread is not serviced. If I do the same with SAIF1 everything works fine. (SAIF1is using another interrupt number)

anyone ho has ever tried using SAIF2 on an iMX233 or any suggestions to debug the interrupt piece from dma to interrupt controller?

thanks in advance,

Maarten.

Tags (1)
0 Kudos
0 Replies