hi all ,
i am having problem with the P&E BDM-Multilink cable,
when i plug the P&E BDM-Multilink cable to USB port of the CPU the blue LED gets detected and it glows. But when i connect the same to HCS08 board it doesnt get detected with target power ,because the yellow LED will not glow.
i have powered on the target board, then why still problem remains same even i tried with some 20 hCS08 boards.
so inorder to conclude that Multilink has gone bad , i tried the same BDM multilink with HCS12 board , but with it it works fine and its easily able to download the code into the controller . so now where is the problem with the board or with the P&E cable????????????????
pls let me know on this as soon as possible.
Regards
ashwini