i.MX28: robust support for VDD5V only configuration -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28: robust support for VDD5V only configuration -blog archive

588 Views
GraceH
Senior Contributor II

imx-bootlets does not handle VDD5V or DCDC_BATT only sources very well.
We have created a patch to add the most robust support possible for a VDD5V or DCDC_BATT only configuration.
It implies enabling of hardware mechanisms to automatically shutdown when the one configured
source becomes invalid. The default power_prep.c file normal tries to configure the protection
as if two sources might be present and thus in some cases, tries to make some determination as
to what to do in software upon one of the power sources becoming invalid.

 

You can get the patch from freescale.com

 

 

https://www.freescale.com/webapp/Download?colCode=L2.6.35_10.12_5V_SUPPLY_PATCH&appType=license&loca...

Tags (1)
0 Kudos
0 Replies