Samaya Lin

Problem to play mpeg2 video for i.MX53 QSB

Discussion created by Samaya Lin on Feb 3, 2012
Latest reply on Feb 3, 2012 by Samaya Lin

A. Screen settings

     My screen setting is HDMI, 1920x1080, the u-boot settings are:

          set hdmi_1080 'video=mxcdi0fb:RGB24,1920x1080MR-16@60 hdmi di0_primary'
          set bootargs_base 'setenv bootargs console=ttymxc0,115200 hdmi_1080'

 

B. Test video file of mpeg2 video :
     ftp://alright-2:alright1689@alright.com.twalright1689@alright.com.tw,  enter the folder i.MX/test_video, 908001.vob, 908002.vob

 

C. Test environment :

     a. lucid image from L2.6.35_11.01.00_ER_images_MX5X.tar.gz, rootfs.tar.bz2

     b. linux kernel 2.6.35 built from LTIB L2.6.35_11.01.00_ER_source_bundle

     c. linux kernel 2.6.35 built from LTIB L2.6.35_11.09.01_ER_source_bundle.tar.gz

 

D. Test procedure :

     gplay [test video filename]

 

E. Test result :

     a. (lucid image) : The video files can be playback, however, the screen will turn to black sometime with IPU error message prompted. After a few seconds, the video will appear on screen again.

          mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00080000

 

     b. & c. (built from ltib) : The video files can not be playback normally, with VDI split not support message, and the frame rate only has fps:8, no video on screen at all.

          video4linux video16: VDI split has not supported yet.
          [Playing  ][Vol=01][00:00:01/00:02:53][fps:8]

 

Is there anybody know how to let these video play normally without screen turn to black ? Thanks.

Outcomes