i.mx53 tab is not booting after flashing the kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 tab is not booting after flashing the kernel

601 Views
sivakumar1z
Contributor I

Hi all,

I am having a freescale imx535 processor based tablet manufactured by richtechie, Chinese manufacturer. It has android 2.3.3 in it.

From the device info i found it has freescale kernel and android.

I downloaded the android source from freescale website, I used imx5_android_defconfig. I compiled the source. I updated the uImage using android recovery and sdcard,

I got the message update was ok.

But when i reboot, The tab is blank and the tab is continuously vibrating.

I am not able to see any log using logcat.

Is there any way to make the tab working.

I tried mfg tool , the tab is detected, but how to flash the kernel using the mfg tool.

Thanks
siva

0 Kudos
2 Replies

486 Views
visakh
Contributor III

siva, you have to get android source for the board which you are using. You may downloaded the source for IMX sabre board. Is your board is same as SABRE in hardware connection and all. Make sure that the hardware(display,wlan,audio etc are same as sabre board) else you have to consult with the manufacturer for its source

0 Kudos

486 Views
daiane_angolini
NXP Employee
NXP Employee

Do you have serial?

I´m not so familiar with mfgtool, but there is a user guide inside the package

0 Kudos