Screenshot-1.pngIfx%20Getting%20Started%20iMX53%20-%20Installing%20Inflexion%20UI%20on%20Linux.pdf
Processing: gst-plugins-ugly
==============================
Processing: gst-ffmpeg
========================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available
WARN: skipping md5sum check for /opt/freescale/pkgs/gst-ffmpeg-0.10.3.tar.bz2, md5 file was not found
Can't get: gst-ffmpeg-0.10.3-relink.patch at ./ltib line 790.
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Fri Jan 20 03:47:40 2012
Ended: Fri Jan 20 03:48:17 2012
Elapsed: 37 seconds
These packages failed to build:
gst-ffmpeg
Build Failed
I am following the steps given in the pdf. However I am getting the following error. I attached the screen shot of the error and the pdf.
Thanks
Hitesh
hi i resolved the issue. i downloaded the relink patch and put in the respective folder still i got error telling relink patch is a garbage file so i downloaded gst-ffmpeg-0.10.3.tar.bz2.md5 and put it in the same folder.
Thanks Vladan
i have set http_proxy and I am able to install packages using "apt-get install" so do u still think its a network issue.
Regards
Hitesh
LTIB is trying to get a package via network and it seems you have no network available for downloading the package...