Now I have patched the android r10.3.1 to the android r10.3 base source .
when I test the dual video function, I found that it can't work
only one screen show the video as well as the screen is flicker
the property setup as below:
[rw.secfb.disable-overlay]: [1]
[rw.SIN_VIDEO_DUAL_UI]: [0]
[rw.DUAL_VIDEO_SIN_UI]: [1]
[rw.SECOND_DISPLAY_CONNECTED]: 1
[sys.SECOND_DISPLAY_ENABLED]: 1
but when I set the [rw.secfb.disable-overlay] to 0, the screen no flicker any more, but still one screen show the video.
Are there any kernel option I haven't choosed.
Thanks you help advance!
Yesterday, I use the mx51 bbg run the r10.3.1 and try to make the dual video output work.
However, the video only output to the primary screen,
Is it impossible archive dual video output on r10.3.1?