CW 6.0 + M5213EVB board (ColdFire MCF5213 CPU) problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 6.0 + M5213EVB board (ColdFire MCF5213 CPU) problem

928 Views
gigi
Contributor I
This is my first time working with CW. When I want to run an application some  errors appears:
 Error : Select port number within valid range
then
PEMicroProtocolPlugin : Can't connect to PEMicro

Those errors appers even when I create a new Project Stationary. The comunication between the EVB board and PE  Hardware seems OK .
 
[CW 6.0 + M5213EVB board (ColdFire MCF5213 CPU) ]
Does anybody have any ideeas how to make them work ? ->
CW 6.0 + M5213EVB board


Labels (1)
0 Kudos
1 Reply

216 Views
J2MEJediMaster
Specialist I
I'm not that familiar with the Coldfire tools, but I'll take a shot at this. What are you using to connect to the board? Those error messages seem to indicate that the communications to the board are messed up. Also, CodeWarrior for ColdFire version 6.3 is available, you may want to consider upgrading

---Tom

0 Kudos