My question is about MMA7260q hardware too, I was reading its datasheet and I have connected mma6270q as indicated by the datasheet but I can't get the right values when x es (+1g) ->2.45v or close to it I only got 1.8-1.9v and when x(-1g) I got 1.4v and is the same in y and z axis why?
I hope you can help me
Hello,
To achieve a +1g voltage of 2.45 volt would require that the device be set to the highest sensitivity of 800 mV/g. It appears that you may currently have the lowest sensitivity setting of 200 mV/g. The nominal output would be 1.85 volt for +1g, and 1.45 volt for -1g, with this setting.
Regards,
Mac