Hello!
I'm running a Qt application on the i.MX53 + 10.1" LVDS display. For styling purpose I use a qlineargradient.
QTreeView {
color: #F0F0F0;
font-family: MS Shell Dlg 2;
font-size: 14px;
font-weight: bold;
background-color: #B9B9B9;
background: qlineargradient(x1: 0, y1: 0, x2: 1, y2: 1, stop: 0 #A9A9A9, stop: 1 #C9C9C9);
border: 1px solid black;
selection-background-color: transparent;
border-image: none;
}
Unfortunately the gradient steps are very distinctiv (see attachment). The second attachment shows the same content on a PC using 32bit graphic.
The LVDS display uses RGB666, so only 18bit is possible.
Is there a way to use qlineargradient that results in same appereance as on the PC? The application would look very simple, if gradients cannot be used.
Thanks für your help!!
Regards,
Rooney