Max Lapshin

CMOS sensor ready to be pluged into iMX 53 quick start board.

Discussion created by Max Lapshin on Dec 6, 2011

Is it possible to buy good CMOS sensor, which is ready to be plugged into the quick start board with i.MX 53 CPU.

 

There is extension slot, but local distributor doesn't have ready sensors with that interface. 

 

Maybe someone has prepackaged ov5642 which can be just plugged without any board development?

Outcomes