Hi,
I have an application in a HCS08GT60 and a bootloader as two separate targets in my CW project. The two outputs are then merged into one .sx (.s19) file for download to the target. This al works fine for me; however I would like to be able to debug the complete device with both application and bootloader. Code wise this is no problem since the code is in different sections of the flash. However with the RAM it is different the stack and static ram is located in overlapping sectors (the application needs the entire RAM). is it possible to make a link (linker file) that knows that the bootloader and the Application does not run at the same time and allows for the bootloaders ram and application ram to overlap?
CW08 3.1 5.0 and 5.1
--
Alban Edit: added CW version + target to message subject
Message Edited by Alban on 2007-03-29 12:01 PM
Solved! Go to Solution.