Is there a listing of intrinsic functions available for CodeWarrior (specifically v5.6.1)?
I have seen reference to __labs(), __fabs(), an intrinsic __memcpy() and some rotate functions throughout the documentation, but never a complete list.
I am building for a ColdFire architecture (MCF5271).
--
Alban Edit: please include target and CW version in message subject
Message Edited by Alban on 2007-03-28 08:38 PM
long __labs(long); double __fabs(double); and void *__memcpy(void *, const void *, size_t);
inline_intrinsics Controls support for inline intrinsic optimizations strcopy and strlen. #pragma inline_intrinsics [ on | off | reset ] Remarks In the strcopy optimization, the system copies the string via a set of moveimmediate commands to the source address. The system applies this optimization if the source is a string constant of fewer than 64 characters, and optimizing is set for speed. In the strlen optimization, a move immediate of the length of the string to the result replaces the function call. The system applies this optimization if the source is a string constant. The default value is ON.