Has anyone attempted to render video using the xvideo extension for X11. I am currently working with an imx51 platform that is running the 2.6.31 kernel and associated packages (imx video driver 09.12.00 and ipu library 09.12.00).
For some reason the IPU will not render images at the proper location on screen. The image is properly scaled but always appears at the top left corner (0,0). I have traced through X11, the imx xv driver and the ipu library and I can see that the xvideo driver is calling mxc_ipu_lib_task_init with the proper output params, specify that the video should appear at some arbitrary screen coordinates but the IPU seems to be ignoring the position specified in the output param argument passed to task_init.
Has anyone had any experience with this?
Hm, somebody stated in src/Makefile.am:
NEON_CFLAGS=-march=armv7-a -mfpu=neon -mfloat-abi=softfp -Wa,-mfpu=neon
Changed it to -mfloat-abi=hard and now it passes.
Why are these flags stated explicitely here? They look like the normal CFLAGS?