eric tai

i.Mx51 2nd display issue in Ubuntu (Kernel 2.6.35.3)

Discussion created by eric tai on Oct 15, 2011
Latest reply on Oct 25, 2011 by eric tai

Hi~~All:

 

 

have anyone porting i.mx51 with Ubuntu 10.04?

 

we're porting Ubuntu 10.04 and kernel version is 2.6.35.3.when boot in 2nd display 800x600 16 bit(RGB565).The Ubuntu display was not good.Bt same parameter are work on wince 6.0 and 7.0.

 

 

{
  /* 800x600 @ 60 Hz , pixel clk @ 40MHz  eric */
  "INNOLUX-SVGA", 60, 800, 600, 25000, 210, 40, 12, 23, 1, 1,
  FB_SYNC_CLK_LAT_FALL,
  FB_VMODE_NONINTERLACED,
  0,},

 

 

Eric

Outcomes