SJA

mainline kernel for MX28 EVK ?

Discussion created by SJA on Oct 15, 2011
Latest reply on Jan 24, 2012 by Robert Schwebel

I am trying to get the mainline kernel running on the MX28 EVK.

But I get no output after "Uncompressing Linux... done, booting the kernel."

FSL kernel works fine.

I have tried both linux-3.1-rc4 from kernel.org and git clone git://git.pengutronix.de/git/imx/linux-2.6.git.

Here are the steps I am following:

export CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-linux-
export ARCH=arm
make mxs_defconfig
make KALLSYMS_EXTRA_PASS=1 uImage

[Copy uImage to tftp server, reboot board running u-boot]

 

## Booting kernel from Legacy Image at 42000000 ...
   Image Name:   Linux-3.1.0-rc4
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1989664 Bytes =  1.9 MB
   Load Address: 40008000
   Entry Point:  40008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Outcomes