Running Barebox on i.mx28/karo TX28 module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running Barebox on i.mx28/karo TX28 module

654 Views
ADTeasdale_amee
Contributor I

We are using the TX28 module from Karo (based around the i.mx28) and want to switch to using Barebox as our bootloader. We have successfully compiled Barebox using the TX28 default configuration and can run this successfully from uBoot. We’ve also been able to configure our graphics driver to display a splash screen from Barebox, which is very useful.

 

We now want to replace uBoot with Barebox and cannot work out how to do this. The instructions http://barebox.org/documentation/barebox-2011.05.0/tx28.html say that you also need the ‘bootlets’ archive and ‘elftosb2’, presumably to include the early initialisation code for the i.mx28. We have both of these but do not seem to be able to find any information on how to use them to create a bootable Barebox image.

 

Can anyone provide any information on how to do this?

Tags (1)
0 Kudos
1 Reply

459 Views
fabio_estevam
NXP Employee
NXP Employee

Please post this question on the barebox mailing list ( http://lists.infradead.org/mailman/listinfo/barebox/ )

 

Regards,

 

Fabio Estevam

0 Kudos