RTAI on i.MX255

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTAI on i.MX255

570 Views
RenaᄏAugustoBen
Contributor I

Hi,

 

I'm trying to create an application using RTAI on a i.MX25 board, but I still without any reference showing me that it's possible to do such thing.

I need to apply RTAI on the kernel and embed it on the iMX board.

 

Could someone guide me or help me about some reference?

 

Att,

Renê Benvenuti

Labels (1)
0 Kudos
1 Reply

505 Views
RobertSchwebel
Contributor IV

Rene,

RTAI is simply plain dead. If you need realtime on Linux, you should probably follow the RT-Preempt path. -rt is available for linux-3.0.x, and the MX25 is well supported in the mainline kernel.

Regards,

Robert

0 Kudos